Issue:
Needs to interlock a pair of D40A, DT60A, D50A, D65A, & DT80A
Product Line:
TeSys D Everlink Contactors, limited to D40A, D50A or D65A
Environment:
Products sold and used in the United States
Resolution:
Use the LAD4CM, without electrical interlock. Alternately the LAD9R3 (which combines both the LAD4CM mechanical interlock and LA9D65A69 set of power connections for reversing contactors for motor contro)l.
Note: LC1DT60A and LC1DT80A has no power connectors. Customer will need to wire it themselves.
Released for: Schneider Electric Canada