Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Replacement pieces on a 8903PB lighting contactor

Issue:
What pieces can be replaced on a 8903PB lighting panel board contactor?

Product Line:
8903PB lighting contactors:

Environment:
US Product

Cause:
Parts on this unit may occasionally need to be replaced

Resolution:
Only the contacts and coils on this device can be replaced.

Coils:
120V - 9998PBV02
208V - 9998PBV08
277V - 9998PBV39

Contacts:
9998PB14

Notes:
The 8903 PB contactor has only 1 coil even though it`s a mechanically held device. (1) kit will be all that is needed to order to get the coil/solenoid and rectifier.
Previous versions of this panelboard contactor had dual voltage coils.  This is no longer an option, and none of these coils are still available.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings