Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does Square D offer individual circuit breaker enclosures for the Homeline breakers?
ISSUE:
Are there HOM breaker enclosures like the QO2100BNS?

PRODUCT LINE:
HOM breakers

RESOLUTION:
No, individual circuit breaker enclosures for the Homeline breakers are not available.

However,Square D does offer some small, 2 space load centers for single phase, 3 wire applications that are basically the same size or similar to what an individual circuit breaker enclosure would be. The following catalog numbers are what Square D offers:
1) The HOM24L70F (indoor NEMA 1, flush mount)
2) The HOM24L70S (indoor NEMA 1, surface mount)
3) The HOM48L125GC (indoor NEMA 1, comes with a combination cover for either flush or surface mount)
4) HOM24L70RB (outdoor NEMA 3R)
5) HOM48L125GRB (outdoor NEMA 3R)

Square D also offers a Homeline SPA-PAK catalog number HOME250SPA, which is a small enclosure that comes from the factory with an HOM250GFI breaker installed for single phase, 3 wire applications.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings