Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a CHU365AWK, Series E5(E05) heavy duty safety switch?
Issue:
Current design repair parts

Product Line:
Heavy Duty Safety Switches

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 4055218951 (3 required; arc suppressor assembly is included)
Arc suppressor assembly - 4051270850 (3 required)
Lug Assembly- 4025113650
Line base phase insulator - 4055219301 (2 required)
Line base mounting screws - 4020600901 (2 required per base assembly)
Operating Handle assembly - 4051217251
Mounting screws for operating handle assembly - 2140122242 (2 required)
Washers for operating handle assembly - 2370100220 (2 required)
Door Thumb Screws - 4405043401 (2 required)
Door Thumb Screw retainer washers - 4405043301 (2 required)
Handle knob kit - 4028343550 (the black and red knob at the end of the handle)
Cross bar insulator - 4055217801 (1 required; this is a red, arc shaped piece approximately 8.85" long)
Cross bar insulators - 4055217701 (2 required; these are red, arc shaped pieces approximately 4.20" long)
Dust Shield for Cross bar - 4055215701 (1 requied; this is a red, flat piece approximately 16" long)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings