Issue:
Is the LXD1B7 still functional if the Teflon wrapping has been removed?
Product Line:
IEC Contactors and Starters
Environment:
Tesys D Coils
Cause:
Teflon wrapping removed.
Resolution:
No, it has to stay on the contactor, it is on there for a reason, if it is not on there, should purchase a new one.
Released for: Schneider Electric Canada