Search FAQs
What is the maximum cable distance from an ATV312 drive to the motor?
Issue:
Max. cable distance from an ATV312 to the motor
Product line:
ATV312, Altivar 312, ATV320, Altivar 320
Environment:
All models
Cause:
n/a
Resolution:
The ATV312 shows that an output filter or choke is required for any cable distance between the drive and motor exceeding 164 feet (50 meters). Above 164 feet, there is a change with shielded vs non-shielded.
Shielded cables
From 164 feet to 330 feet (100 meters) you can use the LR filter cell or a motor choke.
Unshielded cables
From 164 feet to 660 feet (200 meters) you can use the LR filter cell or a motor choke.
Max. cable distance from an ATV312 to the motor
Product line:
ATV312, Altivar 312, ATV320, Altivar 320
Environment:
All models
Cause:
n/a
Resolution:
The ATV312 shows that an output filter or choke is required for any cable distance between the drive and motor exceeding 164 feet (50 meters). Above 164 feet, there is a change with shielded vs non-shielded.
Shielded cables
From 164 feet to 330 feet (100 meters) you can use the LR filter cell or a motor choke.
Unshielded cables
From 164 feet to 660 feet (200 meters) you can use the LR filter cell or a motor choke.
Released for:Schneider Electric Canada
Attachment(s)
Explore more
Range:
Explore more
Range: