Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the terminal shields for the PowerPacT L frame circuit breakers?
Issue:
What are the catalog numbers for the L-frame lug covers?

Product Line:
Circuit Breakers

Resolution:
Here are the catalog numbers for the L-frame terminal shields. Each kit contains 1 terminal shield.

For 3 pole breakers:
The short terminal shield is LTSS3P.
The medium terminal shield is LTSM3P.
The long terminal shield is LTSL3P.

For 4 pole breakers:
The medium terminal shield is LTSM4P.
The long terminal shield is LTSL4P.

Please see attached instruction bulletin for additional information.

Schneider Electric Canada

Attachment(s)
EAV68909-1.pdf [1.61 MB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings