Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the FFTK be used to test M2C contacts and the Micrologic trip unit advanced functions and trip history?
Issue:
Using Full Function Test Kit to test M2C Programmable Contacts.

Product Line:
Powerpact and Masterpact breakers.

Resolution:
When using the M2CTEST special adapter, all advanced protections, logging of trips, logging of alarms, activation of alarms and incrementing of the contact wear counter are enabled during the secondary injection test.
This adapter enables trip unit and M2C/M6C functions the FFTK would normally disable and more closely simulating a primary injection test.
See attached instruction bulletin EAV34309 for more information.

Schneider Electric Canada

Attachment(s)
M2C Test Adapter.pdf [295.16 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings