Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the mechanical interlock for NEMA size 3, size 4 for Classes 8702,8736, and 8810?
Issue:
What is the mechanical interlock for NEMA size 3, size 4 for Classes 8702,8736, and 8810?

Product Line:
Class 8702, 8736, and 8810

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
For vertical mounting:  9999SM11

For horizontal mounting:  9999SM12

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings