Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the 4 piece trim kit without door for the HCN23656, I-Line panel?

Issue:
Trim kit without door for the HCN23656

Product Line:
Panelboards

Environment:
I-Line, HCN, MLO, 3 pole

Cause:
Replacement parts

Resolution:
The 4 piece trim kit without door for the HCN23656, I-Line panel  would be part number HCN65TS ( surface)  trim or the HCN65TF (flush).

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings