Issue:
What type of disconnect is used in the Enclosed U-line starters?
Product Line:
Enclosed U-Line Starters - GIC Prodcut
Environment:
US Product
Cause:
The standard LU9APN21, LU9APN22, LU9APN24 are not the units used in this product
Resolution:
The enclosed U-Line Starters use a newer disconnect device:
The LU9APN43 has a black handle, the LU9APN44 has a red handle. The instruction sheet for these devices is attached.
What type of disconnect is used in the Enclosed U-line starters?
Product Line:
Enclosed U-Line Starters - GIC Prodcut
Environment:
US Product
Cause:
The standard LU9APN21, LU9APN22, LU9APN24 are not the units used in this product
Resolution:
The enclosed U-Line Starters use a newer disconnect device:
The LU9APN43 has a black handle, the LU9APN44 has a red handle. The instruction sheet for these devices is attached.
Released for: Schneider Electric Canada