Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between the 2510KO1 and the 2510KO5 manual switches?
Issue:
What is the difference between the 2510KO1 and the 2510KO5 manual switches?

Product Line:
2510 Type K Manual Switches

Environment:
US Product Lines

Cause:
Both are listed as a 2 pole, single phase standard switches with a pilot light

Resolution:
They have different horsepower ratings.

The 2510KO1 is rated for a maximum of 2hp at 115VAC and 230VAC, 3hp at 460VAC and 575VAC; 1hp at 90VDC, 2hp at 115VDC, and 1.5hp at 230VDC.

The 2510KO5 is rated for a maximum of 2hp at 115VAC, 3hp at 230VAC, 7.5hp at 460VAC, 10hp at 575VAC; 1hp at 90VDC, 2hp at 115VDC, and 1.5hp at 230VDC.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings