Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we add a computer to a domain or change domain after Power Monitoring Expert (PME) has been installed?

Issue:
SPM/PME has been installed while the computer was in a workgroup. Computer now needs to be added to a domain or the domain needs to be changed.

Product Line:
Power Monitoring Expert 7.2

Power Monitoring Expert 8.x

Power Monitoring Expert 9.x

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024
Environment:
Power Monitoring Expert Software Installation

Cause:
The computer name is referenced within the SPM/PME software databases and configuration files, there is a concern whether adding/editing the domain can potentially impact the software.

Resolution:
Simply adding/editing the server to the domain will not affect the software, as long as we are only adding/editing an additional name resolution record, not changing the existing one. For example as long as server1 and server1.company.corp.us will both resolve to the server there should be no issues.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings