Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the door kit for the QO160M200PC?
Issue:
QO160M200PC Door Kit.

Produce Line:
Load Centers

Resolution:
The part number for the door kit is QOCDK60.

NOTE: The QO160M200PC comes with a cover that DOES NOT contain a door. Also, please keep in mind the QOCDK60 is ONLY a box top type of door that is ONLY supposed to attach to the front cover on the QO160M200PC load center and goes over the deadfront area ONLY, where the branch breaker handles show.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings