How can we help you today?

Is the XB7EV03BP Pilot Light Rated for 24V AC or DC?

Issue:
Is XB7EV03BP monolithic pilot light modules rated for AC or DC?

Product Line:
Push Buttons and Operator Interface

Environment:
XB7 Monolithic Operators

Resolution:
It is rated for both 24VAC/DC. It can work with both voltage options.