Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the resistance on the 60Hz coil for a NEMA size 2 contactor?
Issue:
What is the resistance on the 60Hz coil for a NEMA size 2 starter?

Product Line:
9998 NEMA AC Magnetic Coils

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
Values are based on 20 degrees C operating temperature:

120V = 17.8 Ohms

208V = 60 Ohms

240V = 71 Ohms

380V = 178 Ohms

480V = 274 Ohms

600V = 800 Ohms

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings