Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the resistance on NEMA size 00, 0, and 1 coils?
Issue:
What is the resistance on NEMA size 00, 0, and 1 coils?

Product Line:
NEMA Magnetic AC Coils

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
At 20 degrees C operating temperature:

12V = .30 Ohms

24V = 1.21 Ohms

120V = 31 Ohms

208V = 110 Ohms

240V = 126 Ohms

277V = 176 Ohms

380V = 310 Ohms

480V = 510 Ohms

600V = 800 Ohms

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings