How can we help you today?

Video: How to add a Powerlogic device connected through a Modbus Ethernet gateway to ION setup?

Product Line
ION Setup
Powerlogic Meters
EGX100, 200, 300, 400

Environment
ION Setup Configuration

Cause
Video walk through demonstrating how to add a Powerlogic or similar device connected through a Modbus gateway in ION setup.
Video also demonstrates how to verify functionality of the device by viewing real time data readings.

Resolution
The following video depicts the process of adding an EGX gateway as a site in ION Setup and then adding a PM820 meter to the site.



For additional information please reference the ION Setup user guide that can be found at the following link.

https://www.se.com/us/en/download/document/7EN02-0293/


Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: