Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the latest firmware of EGX300 and what is new in it?
Issue
What is the latest firmware for an EGX300 and where can it be downloaded?

Product Line
EGX300

Environment
Firmware

Resolution
The current firmware is 4.461.

EGX300 Version 4.461 firmware provides:
Updates:
  • Corrected issue where BCPM/BCM Circuit/Channel Names were not being saved after power cycle
  • Fixed problem where custom devices were not being saved on disk update.
  • Updated PM5000 Energy
  • Updated Sepam 40 Trending
  • Updated Micrologic H Real Time View
The firmware and disk update files can be downloaded from the attached zip file (V4.461.zip).

NOTE: See FA212757 for instructions on how to upgrade the EGX300 firmware.

Schneider Electric Canada

Attachment(s)
v4.461.zip [2 MB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings