How can we help you today?

Can EV charging device features be upgraded after installation in the field?

Issue:
A unit is already installed in the field, and more functionality is requested.

Product Line:
PTEVC - Electric Vehicles

Environment:
Installed units

Cause:
Extra functionality sought after purchase and installation

Resolution:
EV Charging stations are not upgradeable with other options once purchased. For pedestal mounted units, the base unit and feeder requirements are identical, so a single station can be replaced with any dual station as long as another feeder circuit is installed.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings