How can we help you today?

How to Change Test Mode Timeout in ION8600/ION8650 Meter

Issue
The meter stays in test mode for 30 minutes which is the default period.  This time period may not be sufficient and the user may wish to increase it.

Product Line
ION86xx series
ION8600
ION8650

Environment
Designer, advanced meter configuration in ION Setup

Resolution
The timeout period can be changed in Display Options 1 module, 'Test Mode Timeout' setup register:
Default value is 1800 seconds. Follow the steps below to modify the timeout period then send to the meter.

Figure 1. Display options Module

Figure 1. Display options Module

Figure 2.  make changes using Setup Register

Figure 2.  make changes using Setup Register

Schneider Electric Canada
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
  • Product Selectors