Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the PQ features available on the PM8000 replace the PQ functionality of the ION7650?
Issue:
Does the PM8000 provide the same Power Quality features as the ION7650?

Product Line:
PM8000

Environment:
PM8000

Cause:
The PM8000 does not offer the same features as the ION7650. The PM8000 is a Class S, the ION7650 is a class A.

Resolution:
Here are some features that are present on the ION7650 but not the PM8000:
  • Flicker
  • Transient detection not supported
  • Waveform capture sampling rate of 1024 samples/cycle (PM8000 provides 256 samples/cycle currently)
  • Interharmonics, mains signaling and under/overdeviation
Please see the attached meter data sheet for a more detailed comparison of the ION7650 and PM8000 series meters.

Schneider Electric Canada

Attachment(s)
karls-meter-data-sheet.pdf [1.12 MB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings