Issue:
Plug-On Neutral design repair parts
Product line:
QO load centers
Resolution:
Only the parts listed below are considered field replaceable.
RB door/Cover assembly - 4056317350 (includes hinges)
Interior Trim with labels - 4056314001K this part is OBSOLETE, Order part number 4056314001
Interior Assembly - QO142L225PGRBI (main lugs not included)
Neutral Bonding Screw - 4028344850K
Main Lugs kit - QOL225
Interior trim mounting screw - 4020513001K
RB door/cover mounting screw - 2142717161 (2 required)
Main circuit breaker and main lugs keps nut - 2342702001