Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What auxiliary contacts are used for and 8538 or 8539 combination starter?
Issue:
What auxiliary contacts are used for and 8538 or 8539 combination starter?

Product Line:
8538/8539 Combination Starters

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
The same auxiliary contacts that are used for the Type S contactors and starters, are used for the NEMA combination starters.

1 NO = 9999SX6
1 NC = 9999SX7
1 NO & 1 NC = 9999SX8

*These are field convertible

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings