Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the locking components for the NSYS3D12830P?
Issue:
What are the components for the NSYS3D12830P?

Product Line:
Enclosure

Environment:
S3D H1200xW800xD300+chassis enclosure

Cause:
Customer needs to replace the lock.

Resolution:
NSYS3DLG: Shaft guide, this will come with 10. you only need to use 2
NSYAEDLS3DRL- the standard lock replacement
NSYBTAS3D1200- rod assembly - This part is not loaded in the system yet as a repair part as it is rarely needed as a replacement.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings