Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the wire size/range for Main lug kit NFALM8?
Issue:
What is the wire size/range for Main lug kit NFALM8?

Product Line:
NF Panelboard

Environment:
Application

Cause:
Wire size determination

Resolution:
This is an 800A main lug kit for a NF panel and it will accept (3) 4/0 -  500 kcmil AL/CU wires per phase

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings