Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the purpose of the two extra pins on the LR2K series overload relay?
Issue:
What is the purpose of the two extra pins on the LR2K series overload realy?

Product Line:
TeSys K Mini Contactors - GIC Product

Environment:
US Product

Cause:
Product Characteristics, initial setup

Resolution:
Essentially the internal wiring is meant to facilitate a simple wiring scheme between the overload relay and the complimentary contactor.  When the two pins are utilized, one can simply wire a start button in parallel with terminals 13 on the contactor and 95 on the relay.  With this scheme you would also wire a stop button between your line voltage and terminal 13 on the contactor as shown on the attached diagram.  If you do not desire this control, then break off the two links to disable the internal wiring.

Schneider Electric Canada

Attachment(s)
LR2K Wiring.pdf [1.01 MB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings