Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
RM4JA32 Current Limitation
Issue:
What is the current limitation for the RM4JA32?

Product Line:
RM4JA32 Current Monitoring Relay - GIC Product

Environment:
US Product

Cause:
Product Characteristics

Resolution:
Depnding on which monitoring circuit is wired, the limitations are as follows:
3-15A monitoring - 100A for < 3S or 20A continuous
1-5A monitoring - 15A for < 3S or 7A continuous
03-1.5A monitoring - 10A for < 3S or 2A continuous

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings