Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the voltage threshold for shunt trips for circuit breakers?
Issue:
Shunt trip voltage thresholds

Product Line:
Circuit Breakers

Resolution:
The 120 Vac shunt trip threshold is 55% of the rated voltage.
For all other shunt trips for legacy breakers (F, K, L, M, N, and P frames), the threshold is 75% of the rated voltage.
For Powerpact and Masterpact breakers, the threshold is 70% of rated voltage.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings