Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are I line branch feeders considered to be mechanically restrained in the panel ?
Issue:
Breakers held into panel

Product Line:
Panelboards

Environment:
I-Line

Resolution:
All I-Line breakers bolt down to the back panel/interior. In addition there is a magnetic attraction of the breaker jaws to the bus bars. The two features serve as bonafide retaining means . Incidentally there used to be I-Line breakers that also bolted onto the bus, but these are no longer offered ( or are really necessary).

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings