Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement external reset mechanism for an 8536SB, or SC in a NEMA 4, and 4X enclosure?
Issue:
I need a replacement external reset button for a NEMA size 0, and 1 8536 starter.

Product Line:
8903 type LX lighting contactors

Environment:
US Product Lines

Cause:
Can not find it in the Digest

Resolution:
Part numbers needed are the button 30019-114-58 (which includes 9066W1 protective boot required for NEMA 4 applications), and the ring nut 30019-121-01.

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings