Issue
Attempting to access the PME 7.2.2 Web application in a browser yields the following error:
[Error Summary]
HTTP Error 500.21 - Internal Server Error
Handler "PageHandlerFactory-Integrated" has a bad module "ManagedPipelineHandler" in its module list
Product
Power Monitoring Expert 7.2.2
Environment
PME 7.2.2 Web Applications
Cause
.NET was not registered with IIS during the upgrade or re-install.
Resolution
Run the following command in the Windows command line or powershell as administrator to re-install .NET.%windir%\Microsoft.NET\Framework\v4.0.30319\aspnet_regiis.exe -i