Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How do I rename devices and keep all the historical data aligned in Power Monitoring Expert
Issue:
Devices need to be renamed but historical data needs to be aligned with the new names.

Product Line:
Power Monitoring Expert v7.x
Power Monitoring Expert v8.x
Power Monitoring Expert v9.x
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Cause:
In versions prior to PME 7.2, the only way to rename a meter was to right-click it from the Devices section of the Management Console, select 'Configure device', enter the new name, and click 'OK'.  Doing this creates a new database source using the new name.  The historical data would then be split with all data before the name change under the original source name and all data after under the new name.  The method of right-clicking a device and configuring it to change the name is no longer available in PME 7.2 and newer revisions.  When selecting the 'Configure Device' option the Group and Name fields are grayed out and not modifiable.

Resolution:
As of PME 7.2, a native Rename function has been added to the Management Console which addresses the above issue.
To rename a device in PME:
Right-click on the desired device and select "Rename".
The video below demonstrates the process.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings