Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are I Line Combo Panels rated for use with Single phase voltage
Issue:
Can the I Line Combo Panels be used with Single phase voltage?

Product Line:
I Line Combo Panelboards

Environment:
Application

Cause:
Selection confirmation

Resolution:
The I Line combo Panels are listed for 1 phase /3 wire ; 3 phase / 3 wire , and 3 phase / 4 wire , so they can be used for Single phase wiring.

Schneider Electric Canada

Attachment(s)
2013 I Line Combo panel catalog .pdf [1.96 MB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings