How can we help you today?

How to Delete Hierarchy Configuration

Issue
Quickly removing a large hierarchy.

Product Line
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024

Environment
Hierarchy Manager

Cause
To start new content.

Resolution
*Warning: Loss of Data
Performing this operation permanently removes configuration content from the system.  Ensure this operation is necessary before proceeding.  This procedure cannot be undone.


To delete the configuration content:

  1. Open a Command Prompt window and navigate to:  ...\Schneider Electric\Power Monitoring Expert\Applications\Bin
  2. Type HierarchyConfig.exe delete config.  Type 'yes' when prompted.


To confirm the deletion, open Hierarchy Manager. There should be no hierarchy content displayed.

Note: This delete process does not remove virtual meters. To delete virtual meters, use Hierarchy Manager.

Schneider Electric Canada

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: