How can we help you today?

Why isn't COM'X 510 quantity scaling working?

Issue
The configured scaling of custom frames of custom devices takes on integer values. For example, if a scale factor of 1.8 is used to convert Fahrenheit to Celsius , it will take on the integer value of 1 and not perform the conversion.

Product Line
COM'X 510

Environment
Custom device custom frames scaling parameter

Resolution
This issue is fixed in firmware V1.1.45.

Note: See KB FA270261 for help upgrading the firmware on a COM'X 510.

Schneider Electric Canada

Attachment(s)
ComX 510 v1.1.45 Firmware (EBX510).sp1 [41.65 MB]