Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you get Receptacle Plugs installed on I-Line II Bus plugs?
Issue:
I-Line bus plugs with receptacles or outlets installed ?

Product Line:
I Line Busway

Environment:
Products sold in North America

Resolution:
This option is not an available for the I-Line or I-Line II Bus plugs.  A more standard practice for receptacle location, is to have the plug or receptacle installed close to the load.

The requirement for receptacles in a busplug can be found in our PowerBus Busway design, now rated up to 400A. Besides example below other configurations can also be chosen with various receptacles when requested  via the Distributor or Sales Offices.


Bus plug

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings