Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Devices are not logging the most recent data in PME software

Issue
The real-time data from the devices are shown in Diagrams. However, new data is not being logged into the database.

An error “failed to insert records because 'Insertion rolled back - Could not allocate space for object 'dbo.[DATATABLELOG]'.'IX_[DATATABLELOG]_ID' in database 'ION_Data' because the 'PRIMARY' filegroup is full” is shown in the system log with Source as “LOGINSERTER.[SERVERNAME].”

Product Line

Power Monitoring Expert 7.2

Power Monitoring Expert 8.x

Power Monitoring Expert 9.x

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

SQL Server

Environment
PME

SQL Server 2008 R2
SQL Server 2012
SQL Server 2014



Cause
This error is caused by the database reaching its maximum allocated disk space. Each database is allocated an initial size and allowed to grow according to the pre-set auto growth settings to a specified maximum size.

Resolution
Required to create disk space by deleting unneeded files, dropping objects in the filegroup, adding additional files to the filegroup, or setting auto growth on for existing files in the filegroup.
1. Launch SQL Server Management Studio and connect to the SQL server instance.
2. Expand Databases, System Databases and right-click on ION_Data and select properties from the drop-down menu.
3. Navigate to the filegroups page and ensure that “PRIMARY” is selected as the default filegroup.
4. Select the Files page and review the initial size of the database files that belongs to the “PRIMARY” filegroup.

Image

5. To Setup autogrowth and maximum settings, click on the “…” icon under the Autogrowth /Maxsize column and input a value for File Growth in percentage which is generally between “10%-20%”. Ensure that for Maximum file size, either a sufficient value is entered for “Limited to (MB)” or “Unlimited” is selected.

Image

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings