Issue:
Product Design Features
Product Line:
QO Load Center
Resolution:
The wiring diagram will state to use a 70 A maximum branch breaker OR 10 0A maximum backfed main breaker. When a backfed main breaker is installed, the PK2MB retaining kit must also be used.
This information applies to all the below catalog numbers:
QO612L100F or S
QO612L100DF or DS
QO816L100F or S
QO816L100DF or DS
QO612L100DFCU or DSCU
QO816L100DFCU or DSCU
QO612L100RB or TRB
QO816L100RB
QO612L100RBCU
QO816L100RBCU
QO612L1400TF or TS
QO612L100DTF or DTS
QO816L100TF or TS
QO816L100DTF or DTS
Product Design Features
Product Line:
QO Load Center
Resolution:
The wiring diagram will state to use a 70 A maximum branch breaker OR 10 0A maximum backfed main breaker. When a backfed main breaker is installed, the PK2MB retaining kit must also be used.
This information applies to all the below catalog numbers:
QO612L100F or S
QO612L100DF or DS
QO816L100F or S
QO816L100DF or DS
QO612L100DFCU or DSCU
QO816L100DFCU or DSCU
QO612L100RB or TRB
QO816L100RB
QO612L100RBCU
QO816L100RBCU
QO612L1400TF or TS
QO612L100DTF or DTS
QO816L100TF or TS
QO816L100DTF or DTS
Released for: Schneider Electric Canada