Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many wires will the 84 space NQ neutral accept?
Issue:
How many wires will the neutral accept in an NQ 84 circuit panel?

Product Line:
NQ panelboards sold and supported in the USA

Environment:
Installation

Cause:
Application/product features

Resolution:
400A and 600A will accept:
(60) #4 - #14,
(22) #6 - #14
(4) 2/0 - #14.

225A will accept:
(90) #4 - #14

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings