Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the SC3042M200PS, series M01?
Issue:
Current Design Repair Parts

Product Line:
Combination Service Entrance Devices

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field repairable:
Meter Cover Assembly - 4056171950
Meter Cover Mounting Screw - 4020513002K (contains 10 screws; only 2 are required)
Utility Pullbox Cover - 4056194550 (includes cover latch)
Utility Pullbox Cover Sealing Screw - X1299
Load Center Cover Assembly - 4056172050 (includes latch and hinges)
Load Center Cover Mounting Screws - 2142217101 (2 required)
Dead Front Interior Trim - 4056170001 (labels not included)
Dead Front Interior Trim Mounting Screw - 4020513002K (contains 10 screws; only 2 are required)
Load Center Interior - MTR10002 (main breaker not included)
Load Center Interior Mounting Screw - 4020510001 (2 required)
Main Breaker - QOM2200VH (mounting screw included)
Main Breaker mounting keps nut - 2342702001 (2 required)
Meter Base - 7329882750 (phenolic base only)
Meter Base Mounting Screw - 2142717200 (2 required)
Meter Socket Jaw - 7329794850 (4 required for complete meter socket; blade guide not included)
Meter Jaw Mounting Keps Nut - 2342702001 (per meter jaw)
Meter Jaw Blade Guide - 4052761901 (per meter jaw)
Meter Jaw with Blade Guide - 7329746450 (4 required for complete meter socket; includes blue blade guide)
Meter Sealing Ring - 2920910001
Main Line Side Phase Lugs - 4025116051 (per phase)
Keps Nut for Main Line Side Phase Lugs - 2342702001 (per lug)
Load Center Cover Hasp - 4056174201
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings