Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the 2601 Drum switches Maintained Forward and Reverse? Are they field convertible?

Issue:
Are the 2601 Drumswitches Maintained Forward and Reverse? Are they field convertible?

Product Line:
2601

Environment:
Drum Switches

Resolution:
Yes, they are. This conversion consists of removing the handle screw and handle, turning the shaft 180 degrees, then replacing the handle and handle screw. The drum switch will now operate momentarily in both forward and reverse. The 2601 AG2S2 and 2601 BG1S4 are maintained in forward with momentary operation in reverse and cannot be field converted.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings