How can we help you today?

PME 7.2 / PME 8.0 - Setup fails at check system step: Check for Valid Versions

Issue
The PME 7.2/8.0 upgrade installer fails at the check system step of the process. The setup type is incompatible and prompts the user to "Check for Valid Versions".

PME 7.2/8.0 Valid Versions Error

Product Line
Power Monitoring Expert 7.2

Power Monitoring Expert 8.0

Environment
SQL Server 2008 R2/2010/2012/2014 Standard/Express

Cause
The installer fails at the check system step as a result of an attempt to upgrade/install an incompatible version of PME.

Resolution
1. Ensure that the Power Monitoring Expert software is being installed on a compatible version of Microsoft Windows.

PME 7.2:
32-bit:
- Windows 7 Professional/Enterprise, SP1
- Windows Server 2008 Standard/Enterprise, SP2
64-bit:
- Windows 7 Professional/Enterprise, SP1
- Windows Server 2008 Standard/Enterprise, SP2, and R2 SP1
- Windows Server 2012 / R2 Standard/Enterprise

PME 8.0:
32-bit/64-bit:
- Windows 7 Professional/Enterprise, SP1
- Windows 8.1 Professional/Enterprise
- Windows Server 2008 R2 Standard/Enterprise, SP1
- Windows Server 2012 Standard, SP1
- Windows Server 2012 R2 Standard
- Windows Server 2016 Standard (64-bit only) (Requires PME 8.2)

2. Ensure that the correct edition of PME is being installed/upgraded from the current version.

Example:

- It is possible to Upgrade from Power Monitoring Expert 7.2 Base Edition to Power Monitoring Expert 8.0 Base Edition.
- It is possible to Upgrade from Power Monitoring Expert 7.2 Data Center Edition to Power Monitoring Expert 8.0 Data Center Edition.
- It is possible to Upgrade from Power Monitoring Expert 7.2 Health Care Edition to Power Monitoring Expert 8.0 Health Care Edition.
- It is possible to Upgrade from Power Monitoring Expert 7.2 Base Edition to Power Monitoring Expert 8.0 Data Center Edition.
- It is possible to Upgrade from Power Monitoring Expert 7.2 Base Edition to Power Monitoring Expert 8.0 Health Care Edition.
- It is not possible to Upgrade from Power Monitoring Expert 7.2 Data Center Edition to Power Monitoring Expert 8.0 Base Edition.
- It is not possible to Upgrade from Power Monitoring Expert 7.2 Health Care Edition to Power Monitoring Expert 8.0 Base Edition.


It is recommended to please upgrade to the latest version of Power Monitoring Expert.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Help Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings
  • Preference Center