Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
HOA and other similar operators with 8538 Combination Starters - Series K
Issue:
What type of HOA operator should be used with an 8538S Combination Starter - Series K?

Product Line:
Combination Starter - GIC Product

Environment:
US Product

Cause:
Product Accessories

Resolution:
The series K combination starter uses circular 30mm operators.  The 9999SC8 would be correct for this type of starter.  Older units used the rectangular switches such as the 9999SC2.  These older operators are not compatible with series K combination starters.

For other operators for the 8538 and 8539 combination starters select from the table below:
All devices are class 9999
Starter TypeNEMA 1 KIT Pre-Series KNEMA 1 and 12/3R Kit Series K and Later
Red or green pilot lightPush ButtonSelector SwitchRed or Green Pilot LightPush ButtonSelector Switch
With form F4T (control transformer)StandardStart StopOn OffHand Off AutoOn Off120V 60 HzStart Stop OR On OffHand Off Auto
typetypetypetypetypetypetypetypetype
SB,SCSP12R SP12RSA2SA10SC2SC22SP28R # * (incandescent)
SPL28R (LED - red)
SPL28G (LED - green)
SA3 SC8
SDSP13R SP13R
SESP14R SP14R
SFSP15RSP15R
SG-SJSP28R *SP28R *SA3SA3SC8-

* - the coil voltage must be the same as the pilot light rating. The kit contains on 60 Hz red pilot light control unit 9001KP1R31 - 120V. For other voltages refer to 9001 type KP pilot lghts.
# - Each pilot light kit contains one red and one green lens cap.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings