Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Enclosed D-Line Starter Overloads for Single-phase Applications
Issue:
What overloads are used in the D-Line Enclosed Starter series when a single-phase starter is chosen?

Product Line:
Enclosed D-Line Starters - Enclosed LC1D Starters - GIC Product

Environment:
US Product

Cause:
Product Specifications

Resolution:
These starters use the standard single-phase sensitive overloads.  These overloads are looped at the factory so that they will work appropiately in a single-phase application.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings