Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is in the handle bag assembly 80121-063-50?
Issue:
What is in a Panelboard's handle bag assembly 80121-063-50?

Product Line:
Panelboards

Environment:
Maintenance/Replacement

Cause:
Installation

Resolution:
Handle, latch pawl, mounting hardware, gasketing. Complete handle assy for (1) Nema 3R Handle, see Bill of material, assembly drawing and attached Instruction Bulletin below:

(1)  80022-024-01   MH-WP LOCKING HANDLE
(1)  80106-353-01   NONWELDED WP LATCH PAWL
(1)  23701-00240     LOCK WASHER
(1)  23001-00240     3/8-16 X 5/8  HEX NUT

handle bag

Schneider Electric Canada

Attachment(s)
I Line 80043-615-02 handle assy bulletin.pdf [70.14 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings