Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you land (2) 600 kcmil wire to a PTQ36080G (H, or V) switch?
Issue:
How to wire (2) 600 kcmil to a PTQ36080G (H, or V) switch?

Product Line:
I Line II Busway

Environment:
Installation

Cause:
Options

Resolution:
Yes , since the 1200A and 800A switch enclosures are the same size , wire bending restrictions are not an issue. Using AL800P6K4 lug kit will allow the terminating of (2) 600 kcmil conductors / per phase in the load end of the PTQ switch . The 800A switch normally accepts (3) 500 kcmil with AL800M23K4 lug kit .

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings