Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the ION 8650 cable connecting the I/O Expander option to the meter with breakout panel? and can it be order separate?

Issue
What is the part number for the cable connecting the I/O Expander option to the meter with breakout panel?

Product Line
ION 8650
ION 8600

Environment
ION 8650 Meters
ION 8600

Cause
Need to know if the ION8650 cable connecting the I/O Expander option to the meter with breakout panel can be order separate and the part number.

Resolution
The part number for the ION8650 cable connection the I/O Expander option to the meter with breakout panel is CBL-8X00-BOP-IOBOX
The cable can be order as a separate item.
This cable is 14-pin male Molex connector on one end and 24-pin male Molex connector on the other end.
NOTE: the CBL-8X00-BOP-IOBOX cable is obsolete with no direct replacement

Part Number Breakdown

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings