Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find the proper bolt sizes for the Seismic qualifications for panelboards?
Issue:
Where can I find the proper bolt sizes for the Seismic qualifications for panelboards?

Product Line:
Panelboards

Environment:
Circuit breaker panelboards sold and supported in the USA.

Cause:
Seismic qualifications required

Resolution:
Please refer to the attached Seismic Instruction Label.
All I-Line, NF, NF Column-Width, NQ, NQ Column-Width, NQOB Column-Width, NQOD and
QMB panelboards are seismic qualified when their Type 1 enclosures are mounted at the
locations shown below and use the indicated number of grade 5 steel bolts. NQ and NQOD
panels must also be equipped with bolt-on breakers.

When a side extension is used, all mounting hole locations in the side extension must be used. N represents total number of bolts used for the panel and the side extension.

To be seismic qualified, Type 3R, 3S, 5 and 12 enclosures must be mounted with grade 5 steel bolts and comply with the mounting instructions shipped with the enclosures. Also, NQ and NQOD panels must be equipped with bolt-on type breakers.

Schneider Electric Canada

Attachment(s)
SeismicInstructionLabel.pdf [121.34 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings