Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does the Y029 suffix indicate on a Powerpact L frame?
Issue:
What does Y029 mean on the end of a Powerpact L frame part number?

Product Line:
Molded Case Circuit Breakers

Resolution:
The Y029 indicates medium lug covers on the terminal end (for bus connected breakers). This would increase the height of the breaker to 13.38".
You cannot order a breaker with this suffix. It was developed for a specific OEM. However, you can order LTSM3P and replace the short terminal shield on the breaker with this medium length terminal shield.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings